{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How do I resolve the error: "Application Has Halted Exception: Access Violation ComSystem.dlm:Koohi.cpp:line1078" in the Vijeo Designer simulator when using recipes?

Issue:
How do I resolve the error: Application Has Halted Exception: Access Violation ComSystem.dlm:Koohi.cpp:line1078"


Product Line:
Vijeo Designer


Resolution:
This error occur because the recipe variables are defined as internal variables. If you download to the target, it will
work fine. But if you need to run it in the simulator, you will need to change the Recipe variables to external and not internal type variables.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: