Yes. When programming an M340 or M580 application with Unity Pro, the located REAL variables must be assigned EVEN starting addresses such as %MW2 .%MW4, %MW50 . Addresses using
odd numbers such as %MW1, %MW3 or %MW49 would not be acceptable. Any 32 bit data type would have to follow this regimen. (DINT,DWORD,etc)
Legacy KB System (APS) Data: RESL212622 V1.0, Originally authored by DaSo on 09/27/2013, Last Edited by DaSo on 09/27/2013
Related ranges: Unity Pro - SoCollaborative software
Released for: Schneider Electric Egypt and North East Africa