{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to control BRH motor with 16-trace hyperface encoder by LXM15M?

Goals and Symptoms

Is it possible to control BRH motor with 16-trace hyperface encoder by LXM15M?

Causes and Fixes

Now I finished my tests with the following result:

- In the BRH with a 16 trace Hiperface is a SEK52 inside and with this encoder it is not possible to use the BRH motor in combination with a LXM15.

- But a combination BRH with a 128 trace Hiperface inside (SKS36 encoder) and a LXM15 is possible.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.