{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which firmware version of ILA2E and ILA2E supports the synchronous operation mode for using in TwinCAT-NC?

Goals and Symptoms

Which firmware version of ILA2E and ILA2E supports the synchronous operation mode for using in TwinCAT-NC?

Causes and Fixes

ILA2E and ILE2E supports the synchronous operation mode from firmware version >=V1.015 (>=RS01).
If the device identification plate shows a lower version, the synchronous operation mode are not supported and cannot be updated !!!

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.