{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
what is the maximum current for the R2 relay contacts on all sizes of ATS48 range of soft start

Goals and Symptoms

what is the maximum current for the R2 relay contacts on all sizes of ATS48 range of soft start

Facts and Changes

maximum current
R2 relay
soft start

Causes and Fixes


Characteristics of ATS48 relay :
max voltage : 400Vac (0.2A max)
thermal current : 5A
During life :
AC load
AC1 5A 250V 10E5 cycles (resistor)
AC15-14 : 0.5A (240Vac) 10E6 cycles (contactor)
Cos 0.5 1.8A (240Vac) 10E5 cycles (inductive)

DC load
DC13 : 0.5A (48Vdc) 10E6 cycles (contactor)
L/R 20mS 1.8A (30Vdc) 10E5 cycles (inductive)
minima commutation capacities :
6Vdc 10mA 10E7 cycles (PLC low level)

It's availble for all range.


Legacy KB System (APS) Data: RESL156323 V4.0, Originally authored by on , Last Edited by on
Related ranges: Altistart 48

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.