{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
We have an softstarter ATS48C48Q that is displaying the OCF code. We have been following the instruction on User´s Manual : checking the motor and wiring.

Goals and Symptoms

We have a softstarter ATS48C48Q that is displaying the OCF code. We followed the instruction on User´s Manual : Checking the motor and wire isolation, by-pass circuits testing, and the others recommendations. We did not find anything that explains the situation. The OCF code is displayed randomly, in anytime, inclusive without the RUN command order and without main power supply on L1-L2-L3 . Could you say us what another causes are possible? We already have changed the control board, but the result is the same : the OCF code continues displaying.

Facts and Changes

OCF

Causes and Fixes

In case of OCF error without Run command , there is several potential damage on the component

  • The power board ( bad soldering , component issue on channel measurement current)
  • Thyristor damage
  • Current sensor

These component could be change OR  change completely the product

Schneider Electric Egypt and North East Africa