{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the derating factor used when sizing LH4N for a high number of starts per hour than the standard spec of 360 seconds.

Goals and Symptoms

What is the derating factor used when sizing LH4N for a high number of starts per hour than the standard spec of 360 seconds.

Facts and Changes

LH4N Starts/hour
starting

Causes and Fixes

There is not studies which gives a factor to determine the power of LH4 in an application with high number start/stop per hour upper her electrical characteristics of the product.
The catalogue tell you :
-'' if starting and stopping conditions are severe, or if the starting current must be controlled, it is preferable to use an ATS48 unit''.
- ''beyond this starting duty, the start unit must be derated by one size''.

However , we thinks when the number of start/stop is considerable and it would have been preferable to use a variable speed drive.

Note:  The LH4 softstart family is obsolete. It was replaced by the ATS01 softstart, or in the case of the larger LH4's the ATS22.


Legacy KB System (APS) Data: RESL160232 V1.0, Originally authored by on , Last Edited by on
Related ranges: LH7, LH4

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.