{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What would cause the PRG characters to flash on the central display of a TSX 37 Micro?

The 'write protect switch' set in the 'write authorized' position will cause the PRG characters to flash on the central display of a TSX Micro.

Note: The TSX37 is obsolete and it is recommended to upgrade to the M340 with the x80 I/O contact locals Schneider Sales office or Distributor for more information.

Schneider Electric Egypt and North East Africa