{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the differences between the AS-P810-000 and the AS-P810-001 power supplies?

Issue
Suitable replacement for the P810 power supply.

Product line
984 800 series

Environment
P810 power supply

Resolution
Both models of the P810 operate from either a 115VAC or 230VAC power line. The P810-001 includes a power on/off keyswitch and a front accessible fuse. The P810-000 does not offer these two features. With the exception of the keyswitch and the front-mounted fuse, the two power supplies are identical.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.