{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What values should I expect to see, when using the 140ARI0300, to read Raw Resistance?

Issue

What values should I expect to see, when using the 140ARI0300 to read Raw Resistance?

Product Line

Modicon Quantum

Environment

140ARI0300

Resolution

The data counts are 0-32767 counts converting for which ever range is selected (0-766.66 Ohms or 0-4000 Ohms). I.E. If configuring the range for the channel to 0-766.66 Ohms then 766.66 Ohms = 32767 counts (approx. 42.7 counts per Ohm.)

Schneider Electric Egypt and North East Africa