{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which Magelis HMIs can support with XBTL1001 and which Magelis HMIs do I require XBTL1003M to support?

Issue

Which Magelis HMIs can support with XBTL1001 and which Magelis HMIs do I require XBTL1003M to support?

Product Line

Magelis XBT-L

Environment

XBTL1003M

Resolution

XBTL1001M (the XBTL1000 light software package) only supports the XBTN, XBTH, XBTE, XBTP, XBTHM and XBTPM Alphanumeric Magelis terminals.
XBTL1003M (the XBTL1000 full software package supports the XBTN, XBTH, XBTE, XBTP, XBTHM and XBTPM Alphanumeric Magelis terminals as well as the XBTF Graphical Magelis terminals.

Schneider Electric Egypt and North East Africa