Search FAQs
How do I read or write a program to/from the SY/MAX model 50 controller to the 8005PR4 hand held programmer?
Issue
How do you I read or write a program to/from SY/MAX model 50 controller to the 8005PR4 hand held programmer?
Product Line
SY/MAX
Environment
80005PR4
Resolution
To read a program from the SY/MAX model 50 controller to the 8005PR4 enter the following sequence:
- TRS, READ.
- Once "TRS P T L GO?" is displayed make sure the CPU is halted and a memory pack is installed and then press the ENTR key. "TRS P T L" is displayed during execution.
- When completed "TRS P T L END" is displayed.
To write a program from the 8005PR4 to the SY/MAX model 50 controller enter the following sequence:
- TRS, ENTR.
- Once "TRS L T P GO?" is displayed make sure the CPU is halted and either a 8005MP1 or 8005MP4 CMOS RAM memory pack is installed and then press the ENTR key. "TRS L T P" is displayed during execution.
- When completed "TRS L T P END" is displayed.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: