{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What programming software is required to support the TSX07 Nano PLC?

Article available in these languages: Japanese

Issue
Need to identify the programming software for the TSX07 Nano PLC.

Product line
PL7-07, TSX Nano

Environment
TLXLPL707P40M

Resolution
PL7-07 is required to support the TSX 07 Nano PLC. The part number for a single install is TLXLPL707P40M. Note that this is an obsolete DOS based software. There is no windows based equivalent software.

Schneider Electric Egypt and North East Africa