Search FAQs
Is there any way to add printer types to the list of printers in the UPF editor for Modsoft?
Issue
Is there any way to add printer types to the list of printers in the UPF editor for Modsoft?
Product line
Modicon TSX Micro
Environment
Modsoft
Resolution
No. Modsoft is a DOS based software application. Development of Modsoft has ceased. If the user wants to use a printer other than those listed, the should first try selecting a similar printer type from the available list. If this does not work, the user can print out a straight ASCII text file (MODSOFT.out) and then import that into Word and thereby use Window's printer drivers. It should be noted that the graphics quality suffers greatly when doing this, as such the user may have difficulty reading the prints.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: