{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the Telefast fuse part numbers?

The following fuse part numbers are used in the Telefast 2 PreWired System Connection Interfaces:

Fuse Rating
Part Number
0.125 A
ABE7FU012
0.5 A
ABE7FU050
1 A
ABE7FU100
2 A
ABE7FU200
4 A
ABE7FU400
6.3 A
ABE7FU630

These fuses are fast blow, 5 x 20mm, 250V and have a quantity of 10 per package.

Schneider Electric Egypt and North East Africa