{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
RS485 Communication Wiring Diagram for a Momentum Processor to a Merlin Gerin Digipact DC150

Issue
The purpose of this resolution is to diagram the RS485 wiring for Modbus communications between a Momentum processor and a Merlin Gerin DC150. The RS485 pinout shown in the DC150 User Manual is incorrect.

All Momentum Processors can be used in this application. The following have a builtin Modbus RS485 communications port and do not require a 172JNN21032:
· 171CCC98020
· 171CCC98030
· 171CCS78000
· 171CCC78010


The following Momentum Processors do not have a builtin Modbus RS485 port and requires a 172JNN21032 Option Adapter to work in this application:
· 171CCS70000
· 171CCS70010
· 171CCS76000
· 171CCC76010
· 171CCC96020
· 171CCC96030


The Data Concentrator is:
· Merlin Gerin Digipact DC150

Product Line
Momentum
Merlin Gerin Digipact DC150


Environment


Resolution
RS485 wiring from a Momentum processor (port 2, db9) to a Merlin Gerin DC150.



NOTE: The signal pinouts for the db9 RS485 connector as shown in the Merlin Gerin DC150 User Manual are incorrect. The correct pinouts are shown above.
______________________________________________________________________________

  • RS485 wiring from a Momentum 172JNN21032 Option adapter (port 2, RJ45) to a Merlin Gerin DC150.

NOTE: The signal pinouts for the db9 RS485 connector as shown in the Merlin Gerin DC150 User Manual are incorrect. The correct pinouts are shown above.


Schneider Electric Egypt and North East Africa