{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
DIA6ED1040904EN 3/2005 - Momentum Catalog Contains Incorrect M1E Processor Adapter Descriptions

Issue
The purpose of this resolution is to inform users of Momentum PRODUCTS that an error exists in the processor specifications of the Distributed I/O and Control Modicon Momentum flexible system for distributed I/O and control catalog, part number DIA6ED1040904EN, published 3/2005.

In the 'Selection Guide' on page 8, the description for the M1E Processor Adapters, as shown in the following, is incorrect:

Product Line
Momentum


Environment


Resolution
The following table is the correct description of the M1E Processor Adapter model numbers.


Schneider Electric Egypt and North East Africa