{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Procedure for adding an IP address onto a ProworX32 project for a Momentum 171CCC9x0 x0 M1E processor.

Goals and Symptoms

Procedure for adding an IP address onto a ProworX32 project for a Momentum 171CCC9x0 x0 M1E processor.

Causes and Fixes


· Start up ProworX32
· Open your project


· Select Configuration


· Enter a value into the Config Extension Size (ex. 200)
· This value can be modified later depending on the Config Extension Used value


· Select Configuration Extensions
· Check and highlight TCP/IP
· Enter New IP and Subnet Mask info


· Save project


· Select Communications
· Select which form of connection you currently have to download your project.(Modbus, Modbus Plus or TCP/IP)
· Or enter the PRODUCTS current IP address that is stored on the processor if your just changing to a new IP address.


· Save project


· Open Controller tab
· Select Write All


· Select Write


· Make sure you get the Write to M1 960-20 Complete in the Message Central window


· Select Communications
· Enter New IP address info


· Open Controller tab
· Select Transfer to Flash/EEPROM…


· Select Transfer


· Select Yes to stop the controller

· Make sure you get the Write to M1 960-20 Complete in the Message Central window
· Recycle power to your Momentum processor to make sure all changes were saved


· When the processor powers up and the LAN LED on the processor stays on steady try to ping the new IP address

· Open Controller tab
· Select Start/Stop…

· Select Start

· Make sure you get the Controller is Running in the Message Central window
· Check your logic and make sure all is fine

Schneider Electric Egypt and North East Africa