Search FAQs
Changes form the 'Module Alignment' does not get exported to the .GSD file
Issue
Changes form the 'Module Alignment' does not get exported to the .GSD file
Product Line
Advantys Configuration Software
Environment
Windows 7
Issue
This works as designed. The changes from the 'Module Alignment' will only get exported to symbol
formatted files (i.e., .SCY and .XSY). The reason why the changes do not get exported to a .GSD file
is because 'Module Alignment' only affects the word data stored within the PLC memory. The 'Module
Alignment' is used to align the data within the IO module to a word boundary within the PLC. This allows
the IO data from the slave to have the same layout as that of a Premium Profibus master.
Legacy KB System (APS) Data: RESL191987 V1.0, Originally authored by AlCh on 06/05/2008, Last Edited by AlCh on 06/05/2008
Related ranges: Advantys STB
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: