Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Runtime error 'ERROR Number 75 Path\File access error'.

Issue
Runtime error 'ERROR Number 75 Path\File access error' when trying to
authorize the software. .

Product Line
All Advantys Configuration Software versions

Environment
Windows 7

Resolution
Runtime error 'ERROR Number 75 Path\File access error' gets returned when trying to
authorize the software.

Advantys configuration run-time error


The reason that this happens is because

  • The software is installed under the ...\Program Files folder and the user may not have full
administrative security rights for writing to the folder or sub folders.
  • Access to the installation folder is being blocked by a firewall (i.e., Norton Internet Security,
McAfee Security Suite, etc).

If the software is installed in the ...\Program Files folder, provide the user with full access to the folder by
using the following steps:
  • Right click on Advantys folder and select 'Properties'
  • Click on the 'Security' tab.
  • Click on the 'Full control' checkbox under the 'Allow' column to provide the access to the folder.
Advantys properties



If the above steps are followed and the error still occurs, check the security permissions:

To check the security permissions:
  • Right click on Advantys folder and select 'Properties'
  • Click on the 'Security' tab.
  • Click on 'Advanced'.
Advantys Properties
 
  • Click on 'Permissions' tab.
  • Click on the users name to highlight it.
  • Click on 'Edit'.
Advantys security settings
 
  • Check to see if they have permission to make administrative changes.
  • If the user does not have permission, click on the 'Full control' checkbox under the 'Allow' column to
provide the access to the folder.
Advantys permission entry


If the above steps are followed and the error still occurs, check to see if the firewall, antivirus or
antispyware software is blocking the access to the folder.
 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: