{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
RS485 pinout for the ATS48 to the TCESQM113M13M

Issue
RS485 pinout for the ATS48 to the TCESQM113M13M

Product Line
TCESQM113M13M

Environment
Windows 7

Resolution
The following RS-485 pinout can be used to connect the ATS48 to the TCESQM113M13M

ATS48 TCESQM113M13M

Pin 4 --------------------------- Pin 4
Pin 5 --------------------------- Pin 5
Pin 8 -------------------------- Pin 8

|---- Pin 6
jumper
|----- Pin 8

Schneider Electric Egypt and North East Africa