Goals and Symptoms
Zelio Analog:
Does galvanic isolation between input (Icom, I1, I2, I3) and output (OPG, Io1, Io2, Vo) device?
Facts and Changes
RMC
Zelio Analog
Causes and Fixes
In the Zelio Analog range, the RMCL55BD, RMCV60BD, RMCA61BD contains isolated modules. The isolation value is about 1.5 Kv.
Legacy KB System (APS) Data: RESL198220 V1.0, Originally authored by LaBe on 04/03/2009, Last Edited by LaBe on 04/03/2009
Related ranges: Zelio analog
Released for:Schneider Electric Egypt and North East Africa