{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Maximum Number of I/O Modules in an STBNIP2212 Island Segment

Issue
The purpose of this Resolution is to inform users of Advantys STBNIP2212 Ethernet NIMs that the specification for "addressable modules supported" per segment is incorrect.


Product Line
Advantys STBNIP2212


Environment


Resolution
The STBNIP2212 Applications Guide, part number 31003688, states the 'addressable modules supported' per segment is 16. This number is incorrect.

Although up to 6 segments can configured in an island, there is no limitation to the number of I/O modules in a segment. The only limitation is the maximum number of I/O modules in an island is 32.

Schneider Electric Egypt and North East Africa