Search FAQs
Cannot download to the STBNIP221 after updating to version 2.71
Issue
Cannot download to theSTBNIP221 after updating to version 2.71
Product Line
STBNIP2212
Environment
Windows 7
Resolution
This could happen if the application was created in an older version of the Advantys Configuration Software
and that same version is being used to perform the download.
To resolve the problem:
- Update to the latest version of the Advantys Configuration Software.
- Open the project.
- Click on 'File\Save' to save the project.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: