{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the % voltage drop on the sinus filter both full load and other load?the data in catalog is less than 10%,not note the load,

Goals and Symptoms

What is the % voltage drop on the sinus filter both full load and other load?the data in catalog is less than 10%,not note the load,

Facts and Changes

ATV71

Causes and Fixes

About the voltage drop, the sinus filter is only a inductance the calculation is base of LWI.
L value of inductance
W value of frequency
I value of current.
10% is calculated for M3 at 100 Hz.


Legacy KB System (APS) Data: RESL202270 V1.0, Originally authored by GiVa on 05/12/2010, Last Edited by GiVa on 05/12/2010
Related ranges: Altivar 71

Schneider Electric Egypt and North East Africa