{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to adjust the request packet interval (RPI) on an Ethernet IP slave.

Issue
How to adjust the request packet interval (RPI) on an Ethernet IP slave.

Product Line
TSXETC100, 140NOC771100

Environment
Windows 7

Resolution
The request packet interval (RPI) for an Ethernet IP slave device is configurable using the following
steps.

  • Double click on the 'Ethernet/IP' icon to open the Ethernet IP Configuration Tool,
Ethernet IP configuration tool
  • Double click on the slave device to open the slave properties configuration window.Slave properties configuration
  • Click on 'Connections'.
  • Click on 'General'
  • Double click on 'Request Packet Interval'.
Reset packet interval
  • Change the value in the textbox in the 'Setting' section of the window.
  • Click 'OK'.
Request packet interval (RPI)
  • Click 'OK' to close the slave properties configuration window.
  • Click on 'Save' to save the changes.
Save configuration

Schneider Electric Egypt and North East Africa