{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Expression Blend4 web page does not correctly display INT or DINT values being modified.

Issue
Expression Blend4 web page does not correctly display INT or DINT values after being modified.

Product Line
'BMXNOE0110' and 'TSXETY5103'.

Environment
Windows 10

Resolution
If a change is made to an Expression Blend4 application and it is transferred to the Factorycast
SOAP supported module ('BMXNOE0110' or 'TSXETY5103'), the web page may sometimes display
an error (red circle with an exclamation mark).

The problem is related to the Internet Explorer behavior. It is not Web Designer issue. whenever a
change is made to an existing Blend web page, the historical cache (Temporary Internet files) must
be cleared.

The problem can be resolved by refreshing the web page or clearing the cache in Internet
Explorer using the following steps.

  • Click on Tools\Internet options .
  • Click on General .
  • Click on Delete under Browsing history .
  • Select Temporary Internet files .
  • Click on the Delete button.
  • Click on OK to close the Internet options window.



Legacy KB System (APS) Data: RESL204596 V1.0, Originally authored by AlCh on 03/01/2011, Last Edited by AlCh on 03/01/2011
Related ranges: Modicon M340

Schneider Electric Egypt and North East Africa