Search FAQs
NOE311 does not work with the 'MBP_MSTR'
Issue
'140NOE311' module does not work with the 'MBP_MSTR' function block
Product Line
140NOE31100
Environment
Windows 10, Unity
Resolution
If you try to use the 'Read CTE' option for the 'MBP_MSTR' block to read the information from a 'Symax' drop using an
'140NOE31100', the error 7001Hex will get returned.
The reason that the error gets returned is because the '140NOE31100' is not supported on the MBP_MSTR block for
Unity.
The '140NOE31100' will only work with the MSTR function block for the 984 ladder logic in either Modsoft, Concept,
'ProWORX Nxt' or 'ProWORX 32'. It will not work in Unity.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: