{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the replacement for the Twido TWDDRA16RT 16-point Discrete Output Expansion Module?

Issue:
What is the replacement for the TWDDRA16RT?

Product line:
Twido, OTB, TWD, TM2

Cause:
Product obsolescence.

Resolution:
The replacement is the Twido TM2DRA16RT 16-point Discrete Output Expansion Module. The Twido is obsolete and has been replaced with the M221 and now the TM2DRA16RT modules are also obsolete and that is now replaces with the TM3DQ16R. This will not work with the Twido's or the OTB"s.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: