Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
What is the replacement for the Magelis XBTF011110 HMI?

Issue
Replacement part number

Product Line
Magelis

Resolution
The recommended replacement is the Magelis HMIGK2310 HMI. The software needed to program this terminal is Vijeo Designer. The application in the XBTF011110 is not compatible with the HMIGKxxxx terminals. You would need to recreate the application in Vijeo Designer.

 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more