Issue:
My DIO clouds are not working when they are attached as part of the RIO / ERIO network, How can a DIO cloud be added?
Product Line:
M580
Quantum
Environment:
Unity Pro
EcoStruxure Control Expert
Resolution:
There are 3 ways DIO clouds can be connected to the RIO / ERIO network.
1.) Connect the DIO cloud to the Service Port on the M580 CPU module or CRA module.
2.) Connect to any port on a NOC or NOS module.
3.) Connect to the specified port on the Connexium Managed switch using the pre-built configuration files.
Refer to the attached manuals for further information.
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Released for:Schneider Electric Egypt and North East Africa