{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to Add a '.dat' formatted loadable to ProWORX Nxt

Issue
How to add a '.dat' formatted loadable t 'ProWORX NxT'

Product Line
'ProWORX NxT'

Environment
Windows 7, 10

Resolution
The following steps can be used to add a custom loadable (e.g. EUCA loadable, etc.) that is in the form of '.dat' to
a '.ProWORX NxT' project.

  • Click on 'Configuration\Configuration'.
  • Click on the 'Loadable Library' tab.
  • Select 'Modicon' in the 'Source of Loadables' section of the 'Loadable Library' tab.
  • Click on Browse:

  • Select the 'EUCA-8.dat'.
  • Click on OK
  • Click on Transfer.
  • Browse for the 'PROWORX.USL'.
  • Click on OK.
  • Click on the "User Loadables' tab.
  • Select the 'EUCA' loadable to select it..
  • Click on the 'Load' button to add the loadable into the project database..
  • Click on 'OK' to close the 'Controller Configuration' window.

Schneider Electric Egypt and North East Africa