{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why can I not configure my KYZ output from the CM4000 display?
Issue
User cannot configure the KYZ output from the CM4000 remote display

Product Line
Circuit Monitor 4000 Series

Environment
PowerLogic Power Metering

Cause
Prior to firmware v10.34, the meter would not allow the user to configure the KYZ output from the remote display

Resolution
To use the remote display for KYZ configuration, upgrade the firmware on the CM4000 to a version later than v10.34. FOr instructions upgrading the firmware on a CM4000 meter, please follow the procedure listed in FA237920.

Schneider Electric Egypt and North East Africa