Issue
User wants to use three phase 120V L-N through a potential transformer for control power to the CM4000 that is 69V L-N
Product Line
CM4000
Environment
Wiring
Resolution
User wants to use three phase 120V L-N through a potential transformer for control power to the CM4000 that is 69V L-N
Product Line
CM4000
Environment
Wiring
Resolution
Yes, the circuit monitor can be used with line-to-line rated PT's connected line to neutral, which results in a line-to-neutral voltage of 69. |
Released for:Schneider Electric Egypt and North East Africa