{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for PM800 hardware kit?

Issue
What is the part number for PM800 hardware kit?

Product Line
PM800 Series (PM810, PM820, PM850, PM870)

Cause
Customer wants to order connectors for PM800 series meter (like voltage input connector, Power Supply Connector, and ect.)

Environment
Mounting connectors on PM800 series meter

Resolution
The part number for PM800 hardware kit is 63230-500-16.

The Kit contains the following hardware:

1- Meter template for the cutout = part # 63230-500-09
1- KYCS Output/Input connector = part # 63230-500-29
1- RS485 2 wire connector = part # 63230-500-30
1- Control Power Connector = part # 63230-500-31
2- Retainer spring clips for mounting = part # 63230-500-38 (NOTE: This part number is compatible only with integrated display meter only)
1 - 2-Wire RS485 Terminator MCT2W =63230-500-59
1- Voltage input connector = 63230-500-28

Please review document attach along this article which shows pictures of each connectors and where do they mount on PM800 series meter.

Schneider Electric Egypt and North East Africa

Attachment(s)
PM8_Kit_6323050016.zip [487.98 KB]