Search FAQs
Can One Remote Display be Used for Multiple Meters for the CM4000 or CM3000 or PM800 or PM5000 or PM8000
Issue
Viewing multiple devices on one Remote display screen
Product Line
CM3000
CM4000
PM800
PM5000
PM8000
Environment
Hardware Capabilities
Cause
The remote display is tied to only one meter
Resolution
The remote display is intended for use with a single meter. Other standard operator interfaces, such as Magellis, that support Modbus and RS-485 can be used to display data from multiple meters using one of the comm ports on the meter.
Viewing multiple devices on one Remote display screen
Product Line
CM3000
CM4000
PM800
PM5000
PM8000
Environment
Hardware Capabilities
Cause
The remote display is tied to only one meter
Resolution
The remote display is intended for use with a single meter. Other standard operator interfaces, such as Magellis, that support Modbus and RS-485 can be used to display data from multiple meters using one of the comm ports on the meter.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: