{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the screw size and wire size for the CT and PT terminal connections on the PM820 and PM850 meters?
Issue:
A user requires the information of the screw size and wire size, for the CT and PT terminal connections on the PM820 and PM850 meters.

Product Line:
PM800 series meters

Cause:
A user requires the information of the screw size and wire size, for the CT and PT terminal connections on the PM820 and PM850 meters.

Resolution:
The terminal screws are 6-32 standard screws. Each meter is supplied with spade lugs that accommodate 14-16 AWG wire.

Schneider Electric Egypt and North East Africa