{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How many devices are supported on the RS-485 port (COM3) of the ECC21 card in a CM4000 & CM4000T?

Issue
How many downstream devices can be connected to COM3?

Product Line
CM4 ECC21 Card

Environment
COM3 = RS-485 Serial Port

Resolution
This port supports up to 31 devices (without a repeater), since the device that holds the ECC card counts as a device. The limit is up to 63 devices with a repeater.

Schneider Electric Egypt and North East Africa

Attachment(s)
ECC21_Installation_Guide.pdf [1 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: