{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ION 7700: 'Quick Setup' Option Does Not Show on the Display Unit

Issue
The "Quick Setup" option is not available in the "Setup" menu on the ION 7700 display.

Product Line
ION7700

Environment
Front Display

Cause
The meter MGT unit has old firmware. The Quick Setup menu option was implemented in the most recent firmware versions.

Resolution
Upgrade the meter Firmware to the latest version: V220 (See FA212597).

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.