Search FAQs
Can the Energy Meter CT's be swapped from one Energy meter to another Energy meter?
Issue
Can the Energy Meter CT's be swapped from one Energy meter to another Energy meter?
Product Line
Energy meter (EMB and EME series)
Cause
Customer would like to use existing Energy Meter CTs with another Energy Meter.
Environment
Installing Energy Meter CTs.
Resolution
The Energy Meter CTs can NOT be swapped with another Energy meter. Because the CT's are calibrated with the meter as a unit and therefore can only be used with the meter it is shipped with. Plus, both the Energy Meter and its accompanying CTs will have the same Serial Numbers. As a result, it is not possible to swap Energy Meter CT's from one meter to another meter.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: