{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the Energy Meter be mounted more than 20 feet from the CTs?

Product line
Energy Meters (EMB and EME series)

Environment
Energy Meter Installation

Resolution
The energy meters have been tested and verified functionality with the CTs mounted up to a maximum distance of 300 feet from the meter using 18 AWG twisted leads with 600V insulation (UL 1015 or equivalent).

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.