{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which meters can be ordered in a High Density Metering (HDM) enclosure?

Product Line
PM5000 series meters, ION7550RTU, ION7550, ION7650, MCM, BCPM, BCPMSC, BCPME, BCPMSCE, CM4000T, iEM3500 series, ION6200 series, PM8000 series, EM4800 series

Environment
Digital Metering

Resolution
Pre-wired enclosures begin with one of the following terms:
"MMU-" Multi-Meter Unit;
"HDM-"  High Density Metering;
"9761C-"  Light Industrial Enclosure;
"9761E-"  Industrial Enclosure; and
"9761M-" Main with Feeders Industrial Enclosure.

MMU - Multi-Meter Unit:
iEM3500 series meters are available from 1 to 24 meters in a single enclosure, NEMA 1
Specific meters are the iEM3455, iEM3465, iEM3555, and iEM3565

HDM - High Density Metering:
PM5000 series meters are available from 1 to 8 meters in a single enclosure, NEMA 1 or NEMA 3R
Specific meters are the PM5110, PM5330, PM5340, and PM5560

9761C - Light Industrial Enclosure:
PM5563RD, ION6200, and PM8244, all remote display meters, are available from 1 to 8 meters in a single enclosure, NEMA 1

9761E - Industrial Enclosure:
MCM (Multi-Circuit Meter) meters are available with and without remote displays, 1 meter enclosure only, in NEMA 12 or NEMA 4X

BCPM (Branch Circuit Power Monitor), BCPMSC (Split-core version), BCPME (solid-core version with Ethernet), and BCPMSCE (split-core version with Ethernet) are available in 42-, 84-, or 128-current transformer versions

6200 (ION6200) meters, 5560 (METSEPM5563RD) meters, 8000 (METSEPM8244) meters, 7550 (ION7550) meters, 7650 (ION7650) meters, and 4000 (CM4000T) meters are available in 1- to 4- meters in an enclosure, NEMA 12 or NEMA 4X

ION8650A, ION8650 B, and ION8650C meters are available in either Form 9/36S or Form 35S, NEMA 3R enclosure

9761M - Main with Feeders Industrial Enclosure:
7550 (ION 7550) meters and 7650 (ION7650) meters are available with 1 ION7xxx series Main meter and from 1- to 8- ION6200 Feeder meters in an enclosure, NEMA 12 or NEMA 4X

Please contact the inside sales team for the most up-to-date information.

Schneider Electric Egypt and North East Africa