{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to FTP to an ION meter without seeing the login screen

Product Line
ION Meters

Environment
FTP

Resolution
To connect to a meter using an FTP connection, the username and password can be included in the FTP connection string. The examples below demonstrate how to use the connection string to connect to a meter with an IP address of 123.45.6.78 using Windows Explorer:

Example 1: Standard Security and the default front panel password of 0:

ftp://0:0@123.45.6.78

Example 2: Advanced Security with user1 and password of 12:

ftp://user1:12@123.45.6.78

Schneider Electric Egypt and North East Africa