{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the minimum firmware requirements for Powerlogic meters in StruxureWare Power Monitoring Expert?
Issue
What is the minimum firmware requirements for Powerlogic meters in StruxureWare Power Monitoring Expert?

Product Line
Powerlogic meters
StruxureWare Power Monitoring Expert 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.0
Power Monitoring Expert 8.1
Power Monitoring Expert 8.2

Environment
Power Monitoring Expert Software Configuration

Resolution
It is strongly recommended to upgrade the firmware to the recommended levels to rule out any potential issues. Below are minimum firmware requirements that SPM/PME will support.

Device TypeFirmware Version(s)
PM810/PM820/PM85010.6
PM87010.7
CM3xxx14.35
CM4xxx14.34
PM7503.02
PM700/PM700P/PM7203.01
MicroLogic H8.261 (Logic2005AF)
MicroLogic P8.261 (Logic2005AF)
MicroLogic ANo change in the last five years
MicroLogic Communications ModuleUse in type A, P, and H = 2.001
CM2050/CM2150/CM2250/CM245217.xxx
CM2350/CM245016.xxx
PM60012.004
PM62012.002
PM65022.7
Momentum PLC D16 (EPSS)1.01
Momentum PLC A8 (WAGES)3.03
Momentum PLC D10 (WAGES)3.03


NOTE: SPM can still support older firmware versions. However, some registers might be supported on those versions; and thus they may cause “n/a” or nonexistent measurement displays.
CM2 OS firmware version 14 (and older) has a Y2K issue that affects correct operation in the software. You should upgrade to the latest version.
Vista diagrams may not open correctly if older firmware versions are used. Contact Technical Support for assistance.

Schneider Electric Egypt and North East Africa