Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Is it possible to configure ring topology with Modbus and Modbus Plus communication networks.
Modbus and Modbus Plus networks support line and star topology only. These networks cannot be configured in ring topology.
However, it is possible to connect the devices in dual cable network topology in Modbus and Modbus Plus networks.
However, it is possible to connect the devices in dual cable network topology in Modbus and Modbus Plus networks.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: