{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

How to calculate the scan time of Hot Stand-By (HSBY) system in Modicon Quantum range.

Considering the Hot Stand-By system, the scan time mainly comes from the addition of three parts:
Part 1: User application logic execution time, with an additional data transfer time from Primary to Stand-By communication load RIO management.
Part 2: Depending on the communication load on Modbus, there will be around 1 or 2 ms needed to answer to Modbus read/write requests coming from Modbus network.
Part 3: The scan time needed for RIO management is 2.5 ms
Example:
For 100kb data to transfer from Primary to Stand-By and user logic execution time being less than 6ms, then the scan time of Part 1 is 15 ms (using last CPU firmware version v2.50 or v2.60). Thus ultimately the average scan time will be roughly 19ms for the given example.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: