Search FAQs
What are the recommended CT part numbers for the EM3500 meters?
Issue
What are the recommended CT (current transducer) part numbers for the EM3500 meters?
Product line
EM3500 series meter
Environment
Current connection with EM3500 series meter
Resolution
Low-Voltage (0-1/3 V) Split Core current transducer part numbers are available as shown in table below:
Part Number Description
What are the recommended CT (current transducer) part numbers for the EM3500 meters?
Product line
EM3500 series meter
Environment
Current connection with EM3500 series meter
Resolution
Low-Voltage (0-1/3 V) Split Core current transducer part numbers are available as shown in table below:
Part Number Description
NOTE: These CTs will only work with the EM35xx series; they will not work with EM35xxA. For CTs that will work with the EM35xxA refer to FA233732. The EM35xx will accept either 1/3 V or 1V secondaries.
Size details shown in table below.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: