{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I get the time stamp information for the minimum or maximum values which I can see from the front panel of the Circuit Monitor Series 2000 ?

You will need System Manager Software to see the time stamp of minimums and maximums in the circuit monitor min/max log. The time stamps for these minimums and maximum are not stored in registers.

Original article #4044

Legacy KB System (APS) Data: RESL182801 V1.0, Originally authored by KBAdPM on 03/15/2007, Last Edited by KBAdPM on 03/15/2007
Related ranges: CM2000

Schneider Electric Egypt and North East Africa