Product Line
ION7650/7550
Environment
Register Writing
Resolution
The meter is locked into a Read-Only mode when the password security is anything other than the default of 0 (zero). To write to an External Modbus control registers requires password security to either be disabled, or set to 0.
Released for: Schneider Electric Egypt and North East Africa