Issue
iisrest can help with many web-based bugs, errors, or issues in the power monitoring expert software
Product Line
Power Monitoring Expert 7.2.2
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0
Power Monitoring Expert 9.1
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Environment
Windows
Command Prompt
Intranet Information Services
PME Web Applications
Resolution
- Open the Command Prompt. Click on Start > All Programs > Accessories > Command Prompt
- Once the Command Prompt window opens, type 'iisreset' (without quotes) and then press Enter
- Once the message "Internet services successfully restarted" is displayed, close out of the Command Prompt
Released for: Schneider Electric Egypt and North East Africa